Part Number: TUSB320LAI
Other Parts Discussed in Thread: TUSB320LI, TUSB320
Hi Team,
Our customer would like to use TUSB320LAI but this device is out of stock.
Therefore, their choices are TUSB320 and TUSB320LI.
I refer to the following E2E thread and have some questions.
------
[Q1]
Feature: Current Detection through GPIO
TUSB320: Yes. Can't detect change in current advertisement unless cable removal/insertion
TUSB320LI:Yes
TUSB320LAI:Yes
I understand that TUSB320LI and TUSB320LAI can detect change in current advertisement but USB320 can't detect change.
Is my understanding correct?
If correct, where is this mentioned in the datasheet?
------
[Q2]
Feature: Current Detection through I2C
TUSB320: Yes, requires software workaround to detect change in current advertisement.
TUSB320LI:Yes
TUSB320LAI:Yes
I understand that TUSB320LI and TUSB320LAI can detect change in current advertisement without external control but TUSB320 need external control(software workaround).
Is my understanding correct?
If correct, where is this mentioned in the datasheet?
And, could you please let us know about software workaround of TUSB320?
------
[Q3]
Feature: Directed to Disabled State
TUSB320: No
TUSB320LI:Yes
TUSB320LAI:Yes
I understand that TUSB320LI and TUSB320LIA have “DISABLE_UFP_ACCESSORY” and “DISABLE_TERM” but TUSB320 don’t have those.
Does " Feature: Directed to Disabled State" indicate this difference?
------
[Q4]
Feature: DFP waits for VBUS below VBUS_DET threshold before transitioning from AttachWait.SRC to Attached.SRC
TUSB320: No
TUSB320LI:Yes
TUSB320LAI:Yes
I understand that content of “VBUS_DET IO Pins (Connected to System VBUS signal)” and “VBUS Detection” are same in each device datasheet.
So, I can't understand the difference between "No" and "Yes".
Could you please let us know the difference and detail information?
------
Regards,
Hide