Part Number: DS90UB953A-Q1
Hi Team,
I'm wondering if 953 support interleaved data input like 960 output? Thanks!
Regards,
Cera
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953A-Q1
Hi Team,
I'm wondering if 953 support interleaved data input like 960 output? Thanks!
Regards,
Cera
Hello Cera,
yes, this should be okay as long as both line data have the exact same timing parameters.
Hello Cera,
There are two methods to interleave the transmission of different image data formats: either using the Data Type, or using a different Virtual Channel Identifier
And since those packets are per line, so each line will have different DT or VC-ID. Please see below figures. For more information, please refer to the MIPI CSI-2 Specification Document, Version 1.3, Section "9.13 Data Interleaving".