Hi,
We are using multiple DP83867E PHY on our board. I am currently doing Gigabit Ethernet Compliance Testing on each PHY of the board. I have done the tests on 4 PHYs so far. I just observed that the PHYs are mostly failing on Voltage Point A, and Voltage Point B for Peak Output Voltage (Peak Differential Output Voltage and Level Accuracy Test) for some differential pairs and some would fail on either Voltage difference between Point D and Point A and B and Voltage difference between Point C and Point A and B on top of the other measurements. Also, it is failing on Percentage of eye opening within limit for Transmitter Distortion for some differential pairs. All other tests for gigabit ethernet compliance are passing.
I just want to understand and pinpoint what will be the issue here on the board and how we can improve it or make it pass in the next revision as we plan to redesign the board. Is this a board issue or something on the ethernet compliance test setup that I have to carefully check and perform? I am using R&S test suite for this setup.
BTW. I have performed the gigabit ethernet compliance test as well on the DP83867ERGZ-R-EVM evaluation board with the same setup and those tests are passing except for the pair B transmitted distortion test with and without disturbing signal.
Your input and information would be highly appreciated. Thank you.