Other Parts Discussed in Thread: DS90UB633A-Q1, DS90UB953A-Q1, DS90UB913Q-Q1
Hi,
I have a few questions about Surround View System structure. We are need to combine full HD video streams from 6 cameras and 2 streams from cameras 640x480. We want to use FPD Link III interface for cameras interconnection. Jetson TX2i module will be connected to two DS90UB960-Q1 deserializers. It’s pity, but Jetson have only 3 CSI ports with 4 data lines per each.

1. May we transfer via hub 2 two full HD streams and two low resolution streams via only one TX0 port?
2. How we make a multi-camera synchronization between two FPD Link hubs? Is it possible?
3. May we connect serializer DS90UB633A-Q1 to DS90UB960-Q1 deserializer or we should use chain like: DS90UB633A-Q1 --> DS90UB662A-Q1 --> DS90UB953A-Q1--> DS90UB960-Q1 ?
Regards, Maxim