HI All,
USB 3 device fail to enter into loopback mode
RX: FIO Port25: Rx_5G_Comp-Fail Can’t enter loopback.
Test Method:
The external instrument (M8000) enters from the RX, enters the PCH, and then comes out of the TX to the Connector to form a Loopback
TUSB522P Setting:
EQ1 / EQ2: LOW
OS1 / OS2: High
DE1 / DE2 : Floating.
Do you have any suggestion of measurement method?
Or what is the parameter can be adjusted to make Rx_5G_Comp enter loopback?
/Every_Hsiao