Part Number: TUSB7340
Hi Team,
Could you pls help provide the IBIS_AMI module of TUSB7340, not the IBIS module.
My customer need the IBIS_AMI module for simulation.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Cary:
We only have iBIS model which can be down load from ti.com. For IBIS_AMI model, we don't have resource to do it and it's NRND device.
Regadrs
Brian
Cary:
We don't have next generation Host , we only develop redriver for next generation USB device.
regards
Brian
Hi Brain,
Here is FAE Chi, same customer with Cary.
for system application, could you help to double check this scenario?
PCIe2.0: CPU to TUSB7340, pad to pad, insertion loss 2dB @2.5GHz
USB3.0: 1st way: USB7340 to USB, pad to pad 6.5dB @2.5GHz; 2nd way, USB7340 to redriver, pad to pad 8dB @2.5GHz
BR
Chi
PCIe2.0, 2db loss should be ok.
USB3: you can have 10db on TX with type-A, so both way works.
for type-C, 2nd way works
Regards
Brian