Part Number: SN65HVD230
Hello i have a SN65HVD230. I try to make it work in standby mode:
1. set the SN65HVD230 into standby mode by pulling the Rs pin to HIGH. -> works, i can see 10mA less power draw.
2. wait for a CAN message in standby mode. -> doesn't work. I never receive anything.
How do i correctly use the SN65HVD230 in standby mode? I have setup my MCU to interrupt on a can message but that interrupt is never triggered once we set the SN65HVD230 into standby mode.
i checked and the CAN message gets a NAK. This makes sense as in standby mode we cant send an ACK. But for the ACKto be sent i would have to somehow notice the message in the first place. If i never know that a message is sent how can i set the SN65HVD230 into normal mode so that i can send an ACK? The interrupt is never triggered!
So my problem is that i am pulling the Rs pin to HIGH so the SN65HVD230 goes into standby mode but cant receive anything after that.
Receving/Sending CAN messages work when we stay in normal mode by setting the Rs pin to LOW. So i know that it should work if the SN65HVD230 would only listen.