Part Number: ESDS302
Other Parts Discussed in Thread: TPD2E2U06, TS5USBC402, , ESD752
Hello,
My customer is trying to figure out protection for a USB port that has cabling that runs connector as RS232. They want to protect against the possibility of a DC short to RS232 lines that can go down to -13.2V. I looked at a number of ESD devices and was trying to figure out how to calculate the series resistance needed to protect the ESD device from a DC short.
Is the correct method to just figure out the clamping voltage and the current that would occur. Multiply those together for a power rating and check if the part will heat above its rated temperature using the theta JA numbers? I opened a number of ESD device datasheets and none of them have a continuous current rating or anything similar to help figure this out.
I am trying to protect the TS5USBC402 device which has a negative max voltage of 0.5V. So I was thinking about a unidirectional ESD device like the ESDS302 or TPD2E2U06.
Thanks in advance!
John