This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83640: In my PCB, the SPPED light is on and the other two lights are not working

Part Number: DP83640


Dear Engineer:
I am working on a project to achieve PTP1588 clock synchronization using MCU+DP83640. I have drawn the first version of PCB board, and its schematic diagram is shown in the picture. Now, I have encountered some problems, which are described as follows:
1. It is the first time for me to use LWIP for external network connection, so I choose STM32CUBEIDE for configuration;
2. I can't Ping my computer successfully.
3. The SPEED light of DP83640 is on, but the other two lights are not on, I don't know how to solve it.
I hope to get your help. Of course, I will spare no effort to learn the application knowledge of chip and finish the project as soon as possible.
Best wishes!
Picture at this link, https://postimg.cc/zHw6M0Mk
In the pcb, PHY1_PWRDOWN_NTN and PHY1_RESET_N pins are configured to high level by MCU, and PHY1_X1_Tmp pin is an OCXO of 25MHz. I would like to configure DP83640 in MII mode