Part Number: DS250DF410
Other Parts Discussed in Thread: TUSB1104, TUSB1146
Dear Team,
Please recommend Type-C USB 3.2 G2 (10Gbps) Re-timer or Re-driver.
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Can you describe the application, there are a couple different re-drivers that may be a fit. The TUSB1104 is a good candidate for a Host system application.
Regards,
Undrea
Hi Undrea,
The application of our product is Type-C USB 3.2 G2 (10G), but the Type-C does not have to switch to DP function, just USB function only. Could you suggest more solutions? Thanks a lot!
Many Thanks,
Jimmy
Dear Team,
The application of our product is Type-C USB 3.2 G2 (10G), but the Type-C does not have to switch to DP function, just USB function only. Could you suggest more solutions? Thanks a lot!
Many Thanks,
Jimmy
TUSB1146 and TUSB1104 are both recommended devices which can support Type-C USB3.2 (10Gbps).
Hi Fields,
Thanks for your great support!
The application of our product is shown as below figure, and the below list is the trace length of each segment. We are going to mount the redriver at location with redline, do you have any suggestions? Does the TI / TUSB1104 have the ability to handle this application?
I noticed that TI / TUSB1104 is 10 Gbps USB 3.2 x2, but in our application we don't need x2. Do you have other solution which could meet 10 Gbps USB 3.2 only?

Many Thanks,
Jimmy