This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB321: doubts on the CC controller DRP

Part Number: TUSB321

Hi TI Guru

We are looking for designing a USB DRP product and TUSB321 come to our attention as it just need GPIO pin setting.

We are lacking of I2C resources thus this TUSB321 bring my attention.

I have some doubts below hopefully can get your help on these.

1. What happen if TUSB321 DRP connected to another DRP device, example when i set to DRP and connect to laptop type-C which is another DRP? or Tablet?

2. The port role configuration pin, it samples when a reset or power up. What is the reset here mean? is the USB unplug and plug back consider a reset?

3. If TUSB321 not suitable for my above application, can you recommend a replacement that without I2C? 

Thanks in advance.

Best regards,
Alder