Part Number: TUSB2036
Attached is the schematic I put together on the new design.
R49 is DNP
After I connected USB cable to J4 I am not able to read anything on the USB port.
Mostly I don't see any device plugged into the computer.
After checking U9.P9,P13,P17 all the pins are pulled high.
U9.P10,P14,P18 are also help high.
Due to PWRON1 not turning low the data is not being passed along.
Can you please let me know what changes need to be made so U9 pull the PWR pin low?