Part Number: DS64BR111
Hi,
I am using two SATA III ports for two different SSD
SATA III signal is routed via FR4
one SATA III port routed for the length of 5 inches and connected to SSD via redriver second SATA III port routed for the length of 5 inches and using flex cable (16 inches) connected to another SSD via redriver
please suggest the Equalizer and De-emphasis configuration settings