This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: 954 no output

Part Number: DS90UB954-Q1

Hi Expert,

Our customer use 933+954. On the sensor board, they have two different resolution for the sensor, 720P and 960P. For 720P, it can output well but for 954 it has no output. The detailed register list is as below. May you help check what's the possible issue and reason? Thanks.

0x68,0x0,0x68,0x808
0x68,0x1,0x0,0x808
0x68,0x2,0x1e,0x808//0001_1110
0x68,0x3,0x20,0x808
0x68,0x4,0xdf,0x808//1101_1111
0x68,0x5,0x1,0x808
0x68,0x6,0x0,0x808
0x68,0x7,0xfe,0x808
0x68,0x8,0x1c,0x808
0x68,0x9,0x10,0x808
0x68,0xa,0x7a,0x808
0x68,0xb,0x7a,0x808
0x68,0xc,0x81,0x808//1000_0001
0x68,0xd,0xb9,0x808
0x68,0xe,0x8,0x808
0x68,0xf,0x7f,0x808
0x68,0x10,0x0,0x808
0x68,0x11,0x0,0x808
0x68,0x12,0x0,0x808
0x68,0x13,0x0,0x808
0x68,0x14,0x0,0x808
0x68,0x15,0x0,0x808
0x68,0x16,0x0,0x808
0x68,0x17,0x0,0x808
0x68,0x18,0x0,0x808
0x68,0x19,0x0,0x808
0x68,0x1a,0x0,0x808
0x68,0x1b,0x0,0x808
0x68,0x1c,0x0,0x808
0x68,0x1d,0x0,0x808
0x68,0x1e,0x4,0x808
0x68,0x1f,0x6,0x808
0x68,0x20,0x20,0x808//0010_00
0x68,0x21,0x1,0x808
0x68,0x22,0x0,0x808
0x68,0x23,0x0,0x808
0x68,0x24,0x0,0x808
0x68,0x25,0x0,0x808
0x68,0x26,0x0,0x808
0x68,0x27,0x0,0x808
0x68,0x28,0x0,0x808
0x68,0x29,0x0,0x808
0x68,0x2a,0x0,0x808
0x68,0x2b,0x0,0x808
0x68,0x2c,0x0,0x808
0x68,0x2d,0x0,0x808
0x68,0x2e,0x0,0x808
0x68,0x2f,0x0,0x808
0x68,0x30,0x0,0x808
0x68,0x31,0x0,0x808
0x68,0x32,0x0,0x808

0x68,0x33,0x3,0x808//0000_0011
0x68,0x34,0x40,0x808
0x68,0x35,0x1,0x808
0x68,0x36,0x0,0x808
0x68,0x37,0x0,0x808
0x68,0x38,0x0,0x808
0x68,0x39,0x0,0x808
0x68,0x3a,0x0,0x808
0x68,0x3b,0x1,0x808
0x68,0x3c,0x14,0x808
0x68,0x3d,0x6f,0x808
0x68,0x3e,0x0,0x808
0x68,0x3f,0x40,0x808
0x68,0x40,0x0,0x808
0x68,0x41,0xa7,0x808
0x68,0x42,0x71,0x808
0x68,0x43,0x1,0x808
0x68,0x44,0x0,0x808
0x68,0x45,0x0,0x808
0x68,0x46,0x0,0x808
0x68,0x47,0x0,0x808
0x68,0x48,0x0,0x808
0x68,0x49,0x0,0x808
0x68,0x4a,0x0,0x808
0x68,0x4b,0x12,0x808
0x68,0x4c,0x1,0x808

0x68,0x4d,0x3,0x808//0000_0011
0x68,0x4e,0x4,0x808//0000_0100
0x68,0x4f,0x2a,0x808//42MHz
0x68,0x50,0x0,0x808//
0x68,0x51,0x0,0x808
0x68,0x52,0x0,0x808
0x68,0x53,0x0,0x808
0x68,0x54,0x0,0x808
0x68,0x55,0x0,0x808
0x68,0x56,0x0,0x808
0x68,0x57,0x0,0x808
0x68,0x58,0x58,0x808//0101_1000
0x68,0x59,0x0,0x808
0x68,0x5a,0x0,0x808
0x68,0x5b,0xb0,0x808
0x68,0x5c,0xb0,0x808
0x68,0x5d,0x48,0x808//Remote Slave
0x68,0x5e,0x6c,0x808
0x68,0x5f,0x0,0x808
0x68,0x60,0x0,0x808
0x68,0x61,0x0,0x808
0x68,0x62,0x0,0x808
0x68,0x63,0x0,0x808
0x68,0x64,0x0,0x808
0x68,0x65,0x48,0x808
0x68,0x66,0x6c,0x808
0x68,0x67,0x0,0x808
0x68,0x68,0x0,0x808
0x68,0x69,0x0,0x808
0x68,0x6a,0x0,0x808
0x68,0x6b,0x0,0x808
0x68,0x6c,0x0,0x808
0x68,0x6d,0x7f,0x808//0111_1111
0x68,0x6e,0x88,0x808
0x68,0x6f,0x88,0x808
0x68,0x70,0x1e,0x808
0x68,0x71,0x2c,0x808
0x68,0x72,0xe4,0x808
0x68,0x73,0x0,0x808
0x68,0x74,0x0,0x808
0x68,0x75,0x0,0x808
0x68,0x76,0x0,0x808
0x68,0x77,0xc5,0x808
0x68,0x78,0x0,0x808
0x68,0x79,0x1,0x808
0x68,0x7a,0x0,0x808
0x68,0x7b,0x0,0x808
0x68,0x7c,0x81,0x808
0x68,0x7d,0x0,0x808
0x68,0x7e,0x0,0x808
0x68,0x7f,0x0,0x808
0x68,0x80,0x0,0x808
0x68,0x81,0x0,0x808
0x68,0x82,0x0,0x808
0x68,0x83,0x0,0x808
0x68,0x84,0x0,0x808
0x68,0x85,0x0,0x808
0x68,0x86,0x0,0x808
0x68,0x87,0x0,0x808
0x68,0x88,0x0,0x808
0x68,0x89,0x0,0x808
0x68,0x8a,0x0,0x808
0x68,0x8b,0x0,0x808
0x68,0x8c,0x0,0x808
0x68,0x8d,0x0,0x808
0x68,0x8e,0x0,0x808
0x68,0x8f,0x0,0x808
0x68,0x90,0x0,0x808
0x68,0x91,0x0,0x808
0x68,0x92,0x0,0x808
0x68,0x93,0x0,0x808
0x68,0x94,0x0,0x808
0x68,0x95,0x0,0x808
0x68,0x96,0x0,0x808
0x68,0x97,0x0,0x808
0x68,0x98,0x0,0x808
0x68,0x99,0x0,0x808
0x68,0x9a,0x0,0x808
0x68,0x9b,0x0,0x808
0x68,0x9c,0x0,0x808
0x68,0x9d,0x0,0x808
0x68,0x9e,0x0,0x808
0x68,0x9f,0x0,0x808
0x68,0xa0,0x2,0x808
0x68,0xa1,0xf,0x808
0x68,0xa2,0x0,0x808
0x68,0xa3,0x0,0x808
0x68,0xa4,0x8,0x808
0x68,0xa5,0x18,0x808
0x68,0xa6,0x0,0x808
0x68,0xa7,0x0,0x808
0x68,0xa8,0x0,0x808
0x68,0xa9,0x0,0x808
0x68,0xaa,0x0,0x808
0x68,0xab,0x0,0x808
0x68,0xac,0x0,0x808
0x68,0xad,0x0,0x808
0x68,0xae,0x0,0x808
0x68,0xaf,0x0,0x808
0x68,0xb0,0x1c,0x808
0x68,0xb1,0x13,0x808
0x68,0xb2,0x1f,0x808
0x68,0xb3,0x8,0x808
0x68,0xb4,0x25,0x808
0x68,0xb5,0x0,0x808
0x68,0xb6,0x18,0x808
0x68,0xb7,0x0,0x808
0x68,0xb8,0xac,0x808
0x68,0xb9,0x33,0x808
0x68,0xba,0x83,0x808
0x68,0xbb,0x74,0x808
0x68,0xbc,0x0,0x808
0x68,0xbd,0x0,0x808
0x68,0xbe,0x0,0x808
0x68,0xbf,0x0,0x808
0x68,0xc0,0x0,0x808
0x68,0xc1,0x0,0x808
0x68,0xc2,0x0,0x808
0x68,0xc3,0x0,0x808
0x68,0xc4,0x0,0x808
0x68,0xc5,0x0,0x808
0x68,0xc6,0x0,0x808
0x68,0xc7,0x0,0x808
0x68,0xc8,0x0,0x808
0x68,0xc9,0x0,0x808
0x68,0xca,0x0,0x808
0x68,0xcb,0x0,0x808
0x68,0xcc,0x0,0x808
0x68,0xcd,0x0,0x808
0x68,0xce,0x0,0x808
0x68,0xcf,0x0,0x808
0x68,0xd0,0x0,0x808
0x68,0xd1,0x43,0x808
0x68,0xd2,0x94,0x808
0x68,0xd3,0x3,0x808//0000_0011
0x68,0xd4,0x60,0x808//1101_0100
0x68,0x0,0x68,0x808
0x68,0x1,0x0,0x808
0x68,0x2,0x1e,0x808
0x68,0x3,0x20,0x808
0x68,0x4,0xdf,0x808
0x68,0x5,0x1,0x808
0x68,0x6,0x0,0x808
0x68,0x7,0xfe,0x808
0x68,0x8,0x1c,0x808
0x68,0x9,0x10,0x808
0x68,0xa,0x7a,0x808
0x68,0xb,0x7a,0x808
0x68,0xc,0x81,0x808
0x68,0xd,0xb9,0x808
0x68,0xe,0x8,0x808
0x68,0xf,0x7f,0x808
0x68,0x10,0x0,0x808
0x68,0x11,0x0,0x808
0x68,0x12,0x0,0x808
0x68,0x13,0x0,0x808
0x68,0x14,0x0,0x808
0x68,0x15,0x0,0x808
0x68,0x16,0x0,0x808
0x68,0x17,0x0,0x808
0x68,0x18,0x0,0x808
0x68,0x19,0x0,0x808
0x68,0x1a,0x0,0x808
0x68,0x1b,0x0,0x808
0x68,0x1c,0x0,0x808
0x68,0x1d,0x0,0x808
0x68,0x1e,0x4,0x808
0x68,0x1f,0x6,0x808
0x68,0x20,0x20,0x808
0x68,0x21,0x1,0x808
0x68,0x22,0x0,0x808
0x68,0x23,0x0,0x808
0x68,0x24,0x0,0x808
0x68,0x25,0x0,0x808
0x68,0x26,0x0,0x808
0x68,0x27,0x0,0x808
0x68,0x28,0x0,0x808
0x68,0x29,0x0,0x808
0x68,0x2a,0x0,0x808
0x68,0x2b,0x0,0x808
0x68,0x2c,0x0,0x808
0x68,0x2d,0x0,0x808
0x68,0x2e,0x0,0x808
0x68,0x2f,0x0,0x808
0x68,0x30,0x0,0x808
0x68,0x31,0x0,0x808
0x68,0x32,0x0,0x808
0x68,0x33,0x3,0x808
0x68,0x34,0x40,0x808
0x68,0x35,0x1,0x808
0x68,0x36,0x0,0x808
0x68,0x37,0x3,0x808
0x68,0x38,0x0,0x808
0x68,0x39,0x0,0x808
0x68,0x3a,0x0,0x808
0x68,0x3b,0x1,0x808
0x68,0x3c,0x14,0x808
0x68,0x3d,0x6f,0x808
0x68,0x3e,0x0,0x808
0x68,0x3f,0x40,0x808
0x68,0x40,0x0,0x808
0x68,0x41,0xa7,0x808
0x68,0x42,0x71,0x808
0x68,0x43,0x1,0x808
0x68,0x44,0x0,0x808
0x68,0x45,0x0,0x808
0x68,0x46,0x0,0x808
0x68,0x47,0x0,0x808
0x68,0x48,0x0,0x808
0x68,0x49,0x0,0x808
0x68,0x4a,0x0,0x808
0x68,0x4b,0x12,0x808
0x68,0x4c,0x1,0x808
0x68,0x4d,0x13,0x808//0001_0011
0x68,0x4e,0x5d,0x808//0101_1101
0x68,0x4f,0x23,0x808//0010_0011
0x68,0x50,0xff,0x808//1111_1111
0x68,0x51,0x0,0x808
0x68,0x52,0x0,0x808
0x68,0x53,0x0,0x808
0x68,0x54,0x0,0x808
0x68,0x55,0x0,0x808
0x68,0x56,0x0,0x808
0x68,0x57,0x0,0x808
0x68,0x58,0x58,0x808
0x68,0x59,0x0,0x808
0x68,0x5a,0x0,0x808
0x68,0x5b,0xb0,0x808
0x68,0x5c,0xb0,0x808
0x68,0x5d,0x48,0x808
0x68,0x5e,0x6c,0x808
0x68,0x5f,0x0,0x808
0x68,0x60,0x0,0x808
0x68,0x61,0x0,0x808
0x68,0x62,0x0,0x808
0x68,0x63,0x0,0x808
0x68,0x64,0x0,0x808
0x68,0x65,0x48,0x808
0x68,0x66,0x6c,0x808
0x68,0x67,0x0,0x808
0x68,0x68,0x0,0x808
0x68,0x69,0x0,0x808
0x68,0x6a,0x0,0x808
0x68,0x6b,0x0,0x808
0x68,0x6c,0x0,0x808
0x68,0x6d,0x7f,0x808
0x68,0x6e,0x88,0x808
0x68,0x6f,0x88,0x808
0x68,0x70,0x1e,0x808
0x68,0x71,0x2c,0x808
0x68,0x72,0xe4,0x808
0x68,0x73,0x2,0x808//0000_0010  High byte of Line Count
0x68,0x74,0xd1,0x808//1101_0001  low byte of Line Count
0x68,0x75,0xa,0x808//0000_1010  High byte of Line Length
0x68,0x76,0x0,0x808//   	low byte of Line Length
0x68,0x77,0xc5,0x808
0x68,0x78,0x0,0x808
0x68,0x79,0x1,0x808
0x68,0x7a,0xf,0x808//0000_1111 CSI_RX_STS error
0x68,0x7b,0xff,0x808//1111_1111  CSI Error Counter Register
0x68,0x7c,0x81,0x808
0x68,0x7d,0x0,0x808
0x68,0x7e,0x0,0x808
0x68,0x7f,0x0,0x808
0x68,0x80,0x0,0x808
0x68,0x81,0x0,0x808
0x68,0x82,0x0,0x808
0x68,0x83,0x0,0x808
0x68,0x84,0x0,0x808
0x68,0x85,0x0,0x808
0x68,0x86,0x0,0x808
0x68,0x87,0x0,0x808
0x68,0x88,0x0,0x808
0x68,0x89,0x0,0x808
0x68,0x8a,0x0,0x808
0x68,0x8b,0x0,0x808
0x68,0x8c,0x0,0x808
0x68,0x8d,0x0,0x808
0x68,0x8e,0x0,0x808
0x68,0x8f,0x0,0x808
0x68,0x90,0x0,0x808
0x68,0x91,0x0,0x808
0x68,0x92,0x0,0x808
0x68,0x93,0x0,0x808
0x68,0x94,0x0,0x808
0x68,0x95,0x0,0x808
0x68,0x96,0x0,0x808
0x68,0x97,0x0,0x808
0x68,0x98,0x0,0x808
0x68,0x99,0x0,0x808
0x68,0x9a,0x0,0x808
0x68,0x9b,0x0,0x808
0x68,0x9c,0x0,0x808
0x68,0x9d,0x0,0x808
0x68,0x9e,0x0,0x808
0x68,0x9f,0x0,0x808
0x68,0xa0,0x2,0x808
0x68,0xa1,0xf,0x808
0x68,0xa2,0x0,0x808
0x68,0xa3,0x0,0x808
0x68,0xa4,0x8,0x808
0x68,0xa5,0x19,0x808//0001_1001  FCLK fre
0x68,0xa6,0x0,0x808
0x68,0xa7,0x0,0x808
0x68,0xa8,0x0,0x808
0x68,0xa9,0x0,0x808
0x68,0xaa,0x0,0x808
0x68,0xab,0x0,0x808
0x68,0xac,0x0,0x808
0x68,0xad,0x0,0x808
0x68,0xae,0x0,0x808
0x68,0xaf,0x0,0x808
0x68,0xb0,0x1c,0x808
0x68,0xb1,0x13,0x808
0x68,0xb2,0x1f,0x808
0x68,0xb3,0x8,0x808
0x68,0xb4,0x25,0x808
0x68,0xb5,0x0,0x808
0x68,0xb6,0x18,0x808
0x68,0xb7,0x0,0x808
0x68,0xb8,0xac,0x808
0x68,0xb9,0x33,0x808
0x68,0xba,0x83,0x808
0x68,0xbb,0x74,0x808
0x68,0xbc,0x0,0x808
0x68,0xbd,0x0,0x808
0x68,0xbe,0x0,0x808
0x68,0xbf,0x0,0x808
0x68,0xc0,0x0,0x808
0x68,0xc1,0x0,0x808
0x68,0xc2,0x0,0x808
0x68,0xc3,0x0,0x808
0x68,0xc4,0x0,0x808
0x68,0xc5,0x0,0x808
0x68,0xc6,0x0,0x808
0x68,0xc7,0x0,0x808
0x68,0xc8,0x0,0x808
0x68,0xc9,0x0,0x808
0x68,0xca,0x0,0x808
0x68,0xcb,0x0,0x808
0x68,0xcc,0x0,0x808
0x68,0xcd,0x0,0x808
0x68,0xce,0x0,0x808
0x68,0xcf,0x0,0x808
0x68,0xd0,0x0,0x808
0x68,0xd1,0x43,0x808
0x68,0xd2,0x94,0x808
0x68,0xd3,0x5,0x808//0000_0101
0x68,0xd4,0x60,0x808
x

BR,

Elec Cheng

  • Hi Elec,

    What frame rate is being used for these resolutions and do you know the blanking parameters? It looks like the 720p resolution is reporting errors, line length changes, and line count changes. Does the display look as expected? The 960p resolution does not appear to be receiving any packets from the 953.

    Have they tried programming these resolutions in pat gen? It may be a good test to see if the results are the same.

    Regards,

    Darrah