Part Number: HD3SS3412
hi.. Experts,
I want to use hd3ss3412 device as lvds switch.
Is it output at the same logic level when the input is standard LVDS(ANSI/TIA/EIA-644)?
If not, should I change the logic level on the output?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HD3SS3412
hi.. Experts,
I want to use hd3ss3412 device as lvds switch.
Is it output at the same logic level when the input is standard LVDS(ANSI/TIA/EIA-644)?
If not, should I change the logic level on the output?
Best Regards
this lVDS signal itself can pass though. But if you AC blocked on left side, then you need to biased at 1.2v on the other side or LVDS input.
Regards
Brian