Hi!
We are using RGMII and sending 64 byte packets from the MAC to the PHY (TX direction).
When we read the MAC_CFG_1 Register (Address 0x17), we get rmii_ovf_sts = ‘1’ (“RMII fifo overflow indication”)
The bit also re-appears after clearing it during traffic.
But the traffic is still OK!
- Is the rmii_ovf_sts bit for the FIFO in the TX or RX direction?
- Since we are using RGMII (not RMII), is the rmii_ovf_sts bit to be ignored or does it still apply for RGMII?
Best regards,
Steffen Forså