This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] How to read and write Ethernet PHY registers using a Linux terminal?



There are several different tools available in a Linux environment to read and write registers on a TI PHY.  Several of these options are listed below. 

MII read:
This is the only command which can and must be used in U-boot. Stop the autoboot process as shown here, and type the following: 

“mii read {PHY ID} {register address}”
“mii write {PHY ID} {register address} {value}”

Registers 0x0-0x5 can also be used with the mii dump command to see the function of each bit. Use the following syntax: “mii dump {PHY ID} {register address (0-5)}”

PHYtool:
This tool is used post-boot. This tool is already integrated into TI SDK’s but can be downloaded by typing the following “sudo apt-get install -y net-tools”. To use the tool, type the following:

phytool read {Interface}/{PHY ID}/{register address}
phytool write {Interface}/{PHY ID}/{register address} {value}

To print a dump of all registers 0x0-0x1f, you can use the following command: “x=0; while  [ $x -le 31 ]; do printf  "Register 0x%02X = " $x ; phytool read eth0/0/$x  $(( x++ )) ; done”

MDIO-tool:
To install mdio-tool, use the following commands: 

git clone https://github.com/Yannik25/mdio-tool
cd mdio-tool
cmake ./
make
make install 

To use the tool: