Part Number: DS90UB962-Q1
Hi,
Currently, I am using Ti962 deserializer for streaming four same kind of sensors with (1620W x 1284H) and 30fps by using virtual channel concept. It's able to streaming but the frame rate is degrading.
Here I have configured as follows,
1. 800Mbps/lane the input speed going to 953s from each sensor
2. Output transmitter speed configured as 1.66Gbps which is configured through 0x1F register. (This is maximum transmitter speed as per datasheet)...
Is any thing I missed apart from above configurations...
Kindly help on this issue..
Thanks & Regards,
Dinesh Kedar