Hi TI FAE,
千兆以太网DP83TG720设计上要支持睡眠/唤醒功能,INH管脚唤醒的电平只能是3.3V吗?是否可以接到1.8V的GPIO?看描述是OD门输出,外部是否需要接上拉?实际下图参考电路上又有接下拉10k,是否有推荐的GPIO参考电路,当前使用的SOC GPIO是1.8V的
另外请教下,INT在什么场景下才会使用到?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI FAE,
千兆以太网DP83TG720设计上要支持睡眠/唤醒功能,INH管脚唤醒的电平只能是3.3V吗?是否可以接到1.8V的GPIO?看描述是OD门输出,外部是否需要接上拉?实际下图参考电路上又有接下拉10k,是否有推荐的GPIO参考电路,当前使用的SOC GPIO是1.8V的
另外请教下,INT在什么场景下才会使用到?
The INH pin wake-up level can only be 3.3 V. For further details regarding INH and INT, please refer to the DP83TG720S-Q1 datasheet. Thank you!
Sincerely,
Jason Lee