Part Number: SN65HVD233
Other Parts Discussed in Thread: ESD2CAN24-Q1, , ESD2CAN24
Good morning, excuse me for asking these questions but it is the first time that I am going to use CAN in a design and I want to eliminate some doubts:
1) With the SN65HVD233D can I use CAN in 24 volts? I see that the data sheet indicates +-36 volt protection but I don't know if it is enough to say that it is tolerant to that voltage on the bus.
2) If the CAN line to be installed already has terminators at both ends (with split to the GND of the bus), is it necessary to include it in the boards ? I think it is not necessary but I would like to confirm it because I don't know which PCB would be the first and last and if the bus would be extended in the future.
3) The SN65HVD233D will be powered by a source completely isolated from the bus voltage, can I use the GND of the bus (isolated from the GND of the chip) to connect the PES1DCAN diodes? I think it would still fulfill its function as an ESD protector for the CAN lines, but I don't know if it would affect the SN65HVD233D in any way.
4) In some designs a 1Kohm resistor is used between the MCU and D and T of SN65HVD233D, in others instead pull up resistors are put on both lines, in other cases both are done (the datasheet even adds a C to GND for line D) and in other cases nothing is added. What is the Texas recommendation?
Sorry for my bad english and newbie questions. Thank you