Part Number: DS90UB935-Q1
Does the DS90UB935-Q1 FPD-Link interface run at 3Gbps or 4Gbps?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB935-Q1
Does the DS90UB935-Q1 FPD-Link interface run at 3Gbps or 4Gbps?
Although the 935 is described as a 3Gbps serializer device, please note that the lower speed is actually referring to the reduced CSI-2 available bandwidth, not the FPD-Link line rate. The 935 FPD-Link rates match 953 exactly - i.e. the forward channel runs at 4Gbps or 2Gbps depending on the clocking mode. There is no 3Gbps forward channel mode available in 935. There is no need to design a different PoC network for 935 and the channel recommendations are exactly the same between 935/953. The only difference between 935 and 953 is the allowed total CSI-2 input bandwidth. The 935 can accept up to 2.528Gbps (632Mbps/lane or 316MHz CSI-2 clock in 4 lane input mode). If less lanes are used, then the 935 can accept up to 800Mbps/lane, but the total CSI-2 bandwidth must be <= 2.528Gbps. Below is a data rate matrix:
| Serializer |
Deserializer |
Net CSI-2 Data Rate Per RX Port |
| 953 |
954/960 |
3.328Gbps |
| 935 |
936/962 |
2.528Gbps |
| 935 |
954/960 |
2.528Gbps |
| 953 |
936/962 |
2.528Gbps |