Part Number: TCAN1042DEVM
Other Parts Discussed in Thread: TCAN1044A-Q1, TCAN1042G-Q1, TCAN1042GV-Q1
Hi,
I have a TCAN1042EVM but it has TCAN1042Q1 which supports a max CANFD bitrate of 2Mbps.
My requirement is 5Mbps CANFD datarate. And this is offered by the TCAN1042G device. Can I get a silicon part no. of TCAN which i can use/replace on TCAN1042DEVM Si (which mean new Si should be pin compatible with factory installed TCAN1042 device)? (link of same would help)
Also, please help me with settings of jumpers i need to change/update to get 5mbps on this EVM board.
Current jumper settings :
I am providing 5V at Vcc.
JMP6 is disconnected and a 3.3 V is given to pin P5.
JMP1 is connected to PD
JMP5 is open
JMP4 is connected
Both the Jumper 4 and 5 are to be connected to give 60ohm impedance between CANH and CANL.
Thanks,
Shree