This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84: Question about SN64DSI84 LVDS bridge

Part Number: SN65DSI84

Dear Team,

We are using SN64DSI84 in our project and bringing up the LVDS panel right now.

Currently REFCLK is DSI clock(495MHz), and expected LVDS clock is 72MHz.

As data sheet mentioned,  should keep REFCLK_MULTIPLIER to 0 while using 

DSI clock being clock source.

For our case, the clock source setting and video porch setting are already configured well.

But we still need to set REFCLK_MULTIPLIER to X2 to make panel work.

 

Attached SN65 I2C setting.

Can you help to explain this issue?

https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/138/script.sh