Part Number: TPD4E001
Other Parts Discussed in Thread: STRIKE
Hi Team,
In our C2000 evaluation kit, TPD4E001 is used as the protection circuit on DSP's ADC pin, ADC pin's absolute maximum rating is 4.6V.
I am wondering when transient event happens on ADC pin nodes, how will TPD4E001 work?
TPD4E001's Vbr is 11V, which is higher than ADC pin's maximum rating, does it mean that the transient energy will conduct through the high side internal diode to VCC rather than to GND?
Does it mean that the ADC pin voltage will clamp to VCC+ Vforward(0.6V)?,
Please let me know if my understanding is correct, thanks.