Part Number: PCA9546A
Other Parts Discussed in Thread: PCA9517,
Hi
Can you help to review the following cirucit?
We find there is no ACK from slave device.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you review the circuit first?
I will provide the waveforms later
Thanks
Mike
Hi Mike,
PCA9546A:
The schematic pinout seems to match up with the datasheet pinout.
SDA/SCL lines are properly pull-up through resistors to VCC. I do want to make sure that pull-ups are present on pins 12 and 13 on the input side of the PCA9546A. I think they are probably part of a different page in the schematic.
Local decoupling capacitors are present on VCC's.
It is unnecessary to tie address pins to VCC through 10kohm pull-up. These address pins can be directly shorts to VCC or GND.
/RESET is biased.
PCA9517:
The schematic pinout seems to match up with the datasheet pinout.
SDA/SCL lines are properly pulled-up through resistors to VCC.
Local decoupling capacitors present on VCCA and VCCB.
As of now, I am not seeing any glaring issues with the schematic. Per Clemens' request, please provide scope captures of the I2C bus for further examination.
Regards,
Tyler