Part Number: TUSB216-Q1
Dear Team,
1. We'd like to clarify the TUSB216-Q1 SCL1/SDA1internal PU/PD value.
Please help to confirm if below cognition is right ?
I2C mode (default)
SCL1: 500K ohm PD
SDA1: 500K ohm PU
Non I2C mode (default)
CD: 500K ohm PD
SDA1: 1.8M ohm PD
2.IF SDA1/SCL1 both don't use that means PIN3 & PIN4 without connection on schematic for use case,
is that still normal for application ?
Thank you.