This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Alternate for the component : DS26LV31TM



Hi Team,

In our old design,we were using DS26LV31TM line driver.But now it is obsolete.We need to replace this with a alternate.We selected AM26LV31ID this as a alternate and in online also this part number was suggested.

Our Queries.

  1. Voh/Vol of these IC's are not matching.so can we go with AM26LV31ID part or not?
  2. Any other alternative for DS26LV31TM with same voh and vol levels?

Thanks,

Ganesh P

  • Hi Ganesh,

    1. It depends on what receiver you are using - if the differential receiver can read the lower voltages from the driver this part can be can be used.

    2. We have a pretty large section of quad drivers with most of them being RS-422 compliant which would guarantee 2V differential output over 100 Ohms for the operating range - is there any other specs - such as data-rate, voltage supply, etc.. that are wanted if a part change is made?  Please let me know so I can narrow down potential options.

    Best,

    Parker Dodson