Part Number: TCAL6416
Other Parts Discussed in Thread: TCA6416
We do have the TCAL6416RTWR now available. Could you explain the differences ? Could customer use the TCAL6416RTWR instead of the TCA6416RTWR?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frank,
Main differences between these devices is the voltage supply level. TCA has VCCI/VCCP in range of 1.65 V- 5.5 V, while TCAL has 1.08 V to 3.6 V.
TCAL6416 also fixed the /RESET and INT errata that was present with the TCA6416 device.
Customer could use the TCAL6416RTWR as a replacement device if they are okay with the voltage level change.
Regards,
Tyler