Other Parts Discussed in Thread: PCA9306
Hi all,
I am working on the PCA9306, I2C bus voltage shifter and I am facing with a strange behavior.
The master on the I2C bus works at 3.3V and the slave works at 5V.
In the picture attached you can find part of the electrical scheme. Y2 connector is provide the connection with the master board where the 4K7 pull-up resistors are placed.
When I power-up my system the voltage on VREF1 rises to 4.2V.
I tried to remove the PC9306 in order to check that 3.3V LDO is working well, and that is true.
I tried to connect only the VREF2, EN, SDA2, SDL2 and GND and then check the voltage on VREF1: the value found is 4.2V.
I tried to change the value of the pull-up on EN pin (connected to VREF2) and I notice no changes.
I think my
case is similar to this one: http://e2e.ti.com/support/interface/etc_interface/f/390/t/33915.asp
x
Could you please give me and advice in order to solve my problem?
Could be a power-up sequence? (Before VREF2 and then VREF1)
Thank you very much in advance.