Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Hello,
1. What is need for Programming strap circuit.
2. what is usage of strap circuit below image.

Regards
Rajesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rajesh,
1. What is need for Programming strap circuit.
The Programming Straps offer a way to "program" or setup the PHY in whichever mode you choose, instead of having to use software to commit Register Writes.
Essentially, it is a hardware solution to setting up the PHY. With the Strap settings you can choose the PHY Address, MAC Mode, Speed, etc etc.
2. what is usage of strap circuit below image.
In the DP83869, RX_D0 & RX_D1 are 4-Level strap pins. Meaning there are 4 options that they control. In Table 9: 4-Level Strap Resistor Ratio, we give our recommended resistor ratios for Rhi & Rlo to meet the required voltage levels to correctly configure these pins. The figure is an example of what the strapping circuit would look like.
I hope this clears things up for you, good luck!
Regards,
Alvaro