Part Number: DS25CP114
According to the Control Register table on page 16 of the datasheet, the individual outputs can be powered down. It is not mentioned anywhere however what this means:
- Do the outputs go to High-Z?
- Do they go to a fixed value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS25CP114
According to the Control Register table on page 16 of the datasheet, the individual outputs can be powered down. It is not mentioned anywhere however what this means:
Thanks a lot.
Just as a sanity check: the 100 Ohm termination will still be active/present when the output is shut down?
Hi Marjin,
When output is shutdown, output is high impedance in order Kilo ohms not 100 ohm.
Regards,Nasser
Hi Nasser, Marijn wanted to ask in case of output off, which of the following case will be true?
As shown in this image: https://acrobat.adobe.com/link/track?uri=urn:aaid:scds:US:2f764a72-834b-41cf-96b1-3f651b1b8f80
-Aviral
Hi Aviral,
Please attached the image to this case. For some reason i cannot open this pdf file.
Regards,Nasser