Part Number: DS90UB953A-Q1
Dear Mr or Mrs,
I am working on a project, where I need to propagate power through a Deserializer-Serializer channel (DS90UB954 and DS90UB953A).
In the datasheet of the serializer I find this sentence:
I do not understand if 150mA is a physical limit of the filter (regardless of the component choice) or if it is related to suggested components. In addition, I was wondering if there is a current limit due to the cable I use.
The board where I have the serializer has a power consumption of about 2.5W, so to keep power below 150mA I would need to propagate at least 17V DC through the cable.
Can I properly select components to use a 12V instead (about 0.21 mA DC through the cable)?
I still have the choice to select a twisted shilded pair or a coaxial cable. What do you suggest me? is there any advance in using one or the other?
Thank you in advance for your help.