This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS8136: Can you recommend me an upgrade of this chip

Part Number: THS8136
Other Parts Discussed in Thread: THS8200, , THS8135, THS8200-EP

Hi TI

      Customers need RGB to VGA video chips with industrial wide temperature range (- 40 ° to+85 °), which have similar functions to THS8135/THS8136/THS8200, and benchmark the ADV7123 of ADI.

      I find that only THS8136 and THS8200-EP can do so at present, but THS8136 displays do not support the design of new products, and THS8200-EP has a high price.

      Do you have materials that meet customer needs that can be recommended? Can the roadmap of the chip with this function be shared?