Part Number: DS90UB914A-Q1
Hi,
We met a IIC communication problem between 933 and 914. The signal flow is SOC->914->connectors & coax cable->933->ISP->image sensor. Clock signal flow is OSC(42Mhz)->933->ISP(84Mhz PCLK output)->933-> connectors & coax cable->934. But we found that 933 can transfer the image signal flow to 914 but 914 cannot access 933 and other slave devices on camera side. The camera with 933 is normal because it can be accessed by 934. But the 914 device now is abnormal because it cannot communicate with 913 and 914 devices. We captured the local IIC data from the 914 side and found there is NACK when addressing 913(the 7bit IIC address is 5A). And the next operation(write register address) was incorrect, It seems that the data is shifted 1 bit to the left, and then both the SDA and SCL levels become HIGH. You can see the details from the following screenshots:

The hardware design is shown in the following figure:

We tried not to configure any of the 933's registers, forward channel communication is actually normal, but once we start accessing 933 and try to access the registers (read/write), the LOCK signal will be pulled LOW, I don't know what causing this problem and hope some suggestions from you, thanks!