Part Number: ONET4291VA
Does TI have a quad VCSEL driver ? I want to use a driver IC for HDMI Active Optical Cable. There are 4 transmit channels required for HDMI electrical to optical conversion. Also, on the other end, i need quad TIA receiver IC. The modulation of the driver can be NRZ or PAM4. This is for HDMI so the data rate is 10Gbps... Also, does TI provide Bare die ICs so it can be bonded directly to VCSEL ? Thanks