This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: USB8041 USB Hub Enablement

Part Number: TUSB8041

Hi,

i am trying to enable USB Hub 8041 in qnx, and currently not sure what is the initialization sequence specific to the hub like power enable, reset and so on.

Also is the usb xhci compliant or ehci ?

regards

Annamalai

  • Annamalai

    Can you share your design schematic? The TUSB8041 is a four-port USB 3.0 hub. It provides simultaneous SuperSpeed USB and highspeed/full-speed connections on the upstream port and provides SuperSpeed USB, high-speed, fullspeed, or low-speed connections on the downstream ports, so it will support XHCI and EHCI USB host controller.

    Thanks

    David