Part Number: DP83826E
Hi all,
My customer had a question regarding DP83826x.
"
The following table shows the strap resistors that determine the address of the device in the BASIC mode-

Further back in the data sheet it indicates that all 3 of these pins have internal pulldown resistors. I am confused by the Default state of pin 13 being at ‘1’ and not at ‘0’ if there is an internal pulldown resistor on it. I plan to use external pullup resistors to set the address for each of the 4 devices in my circuit to overcome the 10K pulldown resistors as recommended by this section-

Can you please explain why pin 13 is a ‘1’ by default, and also, what is the Mode column representing? Is it referring to the Basic or Enhanced mode or is it referring to the state of the pin with or without the external resistor?