Part Number: TUSB9261
Hello Support,
I need solution to controlling the GPIO10 under Linux with firmware 1.06 to reset the SDD, because the SDD is not at every boot available.
Can you send me a command to use it.
Best regards Iliya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB9261
Hello Support,
I need solution to controlling the GPIO10 under Linux with firmware 1.06 to reset the SDD, because the SDD is not at every boot available.
Can you send me a command to use it.
Best regards Iliya
Hi Iliya,
Unfortunately, we currently do not have any active support for the linux version of our TUSB9261 FW or flashburner.
The best thing I can recommend is that you take a look at these previous E2E threads and see if they fulfill what you are asking for.
Thanks,
Ryan
Hello Ryan,
I don't find a command to reset the SDD in the topics.
My shematic is designed according to TI Demoboard and the GPIO10 is used as enable the SDD.
TI firmware shutt be have the reset option in the firmware.
Please check it or send me the source code of the firmware/driver.
Regards Iliya