Part Number: DP83TC811R-Q1
Hello,
we are using the DP83TC811R-Q1 Low Power Automotive PHY. The Phy has the automatic function to change the polarity if the wires are not correctly connected. We want to know when this happens, which parameter does describe the change of the polarity. In 8.4.12.2 is just described that the auto-polarity correction can be enabled or disabled, but we want it enabled but we want also to see when the auto-polarity is used.
We tried with Register 0x0013 (bit 1 and 9) and Register 0x0475 (bit 13). But the value is not changing to 1. How can i detect that the polarity is wrong? Thanks in advance.