Part Number: PCF8575C
Hi sir,
In the respective application of this IC,pull up resistor values are given as 10K. If we calculate the pull up value according to the equation Rp(max) = tr/(0.8473*Cb) = (300ns/(0.8473*400pf) gives 885ohms,which implies maximum value of pull up is 885. them why 10k is used. The vcc supply for my design is 5V. shall I stick on to 10K?