Hi Team,
DS90UB933 and DS90UB954 are connected by STP cable.
I know that remote access from the 954 to the 933 is possible.
However, in my evaluation, I would like to have remote access from the 933 to the 954.
Is this possible?
If so, what are the register settings required for remote access for both the 933 and the 954?
We will give you the evaluation details as a reference.
Evaluation details
1. Periodically read register 0x36 for 933 to 954.
When IE_CSI_PASS_ERROR of 0x36 becomes "1
2. Apply a digital reset to 933 to 954
(Set DIGITAL_RESET1 in register 0x01 of 933 to 954 to "1")
3. Set the registers 933 to 954 again
(I set the registers according to my usage)
Best regards,