Part Number: DP83822I
Other Parts Discussed in Thread: AM3352
Team,
Two device questions here.
For the T3 of the power up timing, d/s says max value is 200ms. What's the typical value? Is there a counter inside the device for T3?
What if there is external signal to influence it duringT3 period of time? For example, if there is something unexpected behavior happened with AM3352 inside PD. how does DP83822 response if something is happened?


There are 4 modes in device with HW strap setting.
what if the strap voltage is fall in 0.9142V ~ 2.2901V? How does device react if strap voltage is out of this range?