Part Number: SN65DSI83
Other Parts Discussed in Thread: SN65LVDS822, DS90CR288A, DSI-TUNER
Thank you very much for your kind attention.
I am S.Kikuchi from Borderless.
I was able to read/write each register from I2C to the SN65DSI83 and set each register, but the MIPI signal seems to be going to the IC (SN65DSI83).
The MIPI signal seems to be going to the IC (SN65DSI83), but the output signal (LVDS) does not seem to be output.
The SN65DSI8XEVM evaluation board is used to check the operation.
The configuration of the evaluation set we are currently checking has the following specifications.
1. The DSI source is connected to J4 in our currently operating system and outputs data.
2.LVDS signal from J6 is connected to SN65LVDS822 via cable and connected to SONY ECX336B monitor.
3. An I2C host is connected to J10 using an external I2C host (PC).
Monitor (SONY ECX336BF)
Small-size, high resolution 0.23 nHD+ display dots 640 (RGB) × 400 = 0.77M dots
Input interface that supports parallel RGB 24-bit, YCbCr 24-bit and YCbCr 16-bit input
(* Used with RGB 24-bit)
The DSI source is connected to J4 in our currently operating system and is outputting data.
LVDS signal does not seem to be output from J6. (Confirmed by signal).
The LVDS signal from J6 is not connected to the SN65LVDS822.
We will send you a separate document for setting up each register.
Best regardsSN65DSI83RegisterSetting.xlsx