This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320LAI: ID pull-up resistor value

Part Number: TUSB320LAI

Hello,

I found some similar posts, but I want to confirm.
The datasheet recomends to use 200Kohm for the external pull-up resistor on ID pin.
My customer wants to use 220Kohm from E12 standard instead of 200K ohm.
Is it acceptable?

And I believe that this resitor value is valid for all VDD range, 2.7- 5.0-V. Correct?

Regards,

Oba