This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130: FPGA used SN75DP130 as DP to PC converter, but some appear AUX timeout

Part Number: SN75DP130

 Hello,

 One customer confirm DP IP function with FPGA. He used SN75DP130 as DP to PC converter, but some display appeared AUX  timeout. The detailed test results are as following:

1. HP223, DP port1: AUX communication normally, and display is normally lighted.

2.HP224,LG, DP port0: AUX  timeout.

3.Samsung: only displayed once during tests, and other tested results are all AUX timeout.

 1.   LG:N/P amplitude too small, is not compatible with AUX protocal.

             

       2. HP223 port1:work normally

           

        3.HP224 port0(AUX timeout): compared with port 1 above, the differences are marked red circle.

          

Please give me some advice

Best regards

Kailyn