Part Number: TCA6408A
Hello,
Our customer has a question about I2C signal line condition in TCA6408A RESET initialization process. Could you let us know whether you experienced pulling I2C line low during RESET initialization process.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA6408A
Hello,
Our customer has a question about I2C signal line condition in TCA6408A RESET initialization process. Could you let us know whether you experienced pulling I2C line low during RESET initialization process.
Best regards,
Hi Bobby,
Thank you very much for your quick reply.
We could not get our customer exact use case though, would it be possible to let us know following two cases.
1. Device is already powered up then toggle /RESET.
2. during Power up with /RESET=Low.
Best regards,
Hi Toshiro,
1. Device is already powered up then toggle /RESET.
This should be fine, I've never heard of any issues with this situation occur before.
2. during Power up with /RESET=Low.
This should also technically be okay.
There is one case that we've seen some troubles with. It doesn't have to do with the #RESET but instead the power sequencing of TCA64XX. I believe Vccp needs to power up before Vcci or in some cases the SDA can lock until both power supplies are up. I'll need to double check on the power sequence to be sure but we are planning to update the datasheet to state this in the power supply section as well as issue a PCN when the change is made.
-Bobby
Hi Bobby,
Thank you very much. I understood.
Regarding to VCCI, VCCP power sequencing, would you let us know the secure way that will not happened SDA lock condition that are known at this moment.
best regards,
Hi Bobby,
Thank you very much. The customer informed that VCCI and VCCP power up simultaneously, so I suppose this customer does not face on any issue.
Best regards,