Hi All,
We have 2 questions when using TUSB4020BI-Q1.
1. Since we only need the TUSB4020BI-Q1 as a USB 2 HUB, no power switch or SMBus/I2C is needed.
May I know how to configure below pins?
- SCL / SMBCLK (Pin 2) -> Leave unconnected?
- SDA / SMBDAT (Pin 3) -> Leave unconnected?
- SMBUSz (Pin 22) -> Leave unconnected?
- PWRCTL_POL (Pin 21) ->Leave unconnected?
- GANGED / SMBA2 /HS_UP (Pin 35) -> Leave unconnected?
- FullPWRMGMTz /SMBA1 (Pin 36) -> Leave unconnected?
- GRSTz (Pin 11) -> Add 1uf cap to GND?
2. We would try to reduce the power consumption of the IC.
May I know whether TUSB4020BI-Q1 has any power saving mechanism even the I2C and SMBus are not used?
I would also like to know why the current consumption are the same under below 3 conditions(Power-on/Disconnect/Suspend).
And what is the definition of each of them?
Looking forward to your reply.
Thank you.