Part Number: DP83TC811S-Q1
Other Parts Discussed in Thread: DP83TC811, DP83TD510E
Hi,
For a new project I would like to get some answer on the following questions:
- I need a PHY for Ethernet communication between central unit and up to 16 units.
The application is Avionics and the temperature grade of the PHY need to be at least 125C junction
What is your recommendation of such PHY (PHYs) which will have long longevity ?
- I consider using the Automotive PHY DP83TC811S-Q1 since it has the ability to work on single pair based on the 100BASE-T1 standard. However, since the max length between the units can reach up to 60m~80m and I do not need 100Mbps I thought operating it in 10Mbps.
- In that case, can you say surely what will be the range of the cable the DP83TC811S-Q1 can support ?
- If the device is set to 10BASE-T full Duplex using the BMSR register, does it means it will support 10BASE-T on single pair with the standard cable length of 100m ?
- In the data sheet it is written " 100BASE-T1 – IEEE 802.3bw Compliant – OPEN Alliance Qualified – Interoperable With BroadR-Reach and 100BASE-T1 PHYs " What is the meaning of the sentence " OPEN Alliance Qualified " and will keep on interoperability if the rate will be 10Mbps and not 100Mbps ?
- Since the product will have a lot of PHYs, in order to reduce the routing I wish to work in SMII mode.
- Why this mode is SGMII and not SMII (1000M vs 100M) ?
- If I would like to operate the device in 10Base-T and not 100Base-T can I work with SMII/SGMII ?
- What would be the rate of the SMII bus when working in 10BASE-T mode
- It is written that the clock to the PHY (XI pin 5) is 25M in case of MII / RGMII / SGMII and 50M in RMII mode. Is the 25M still true if the unit works in 10BASE-T and not 100BASE-T ?
Thanks,
Avner