Part Number: DP83867IS
Other Parts Discussed in Thread: DP83869
Hi team,
My customer have to estimate the worst case power consumption and thermal.
Could you provide the maximum current for each power rail under below condition?
BTW, why the Channel Utilization is set to 50% in "4 Power Consumption Baseline Data" in below document?
http://proddms.itg.ti.com/stage/lit/an/snla241/snla241.pdf
- SGMII
- Two supply configulation
- VDDIO = 1.8V
- VDDA1P0 = 1.0V
- VDDA2P5 = 2.5V
- Ta max = 85c
- Channel Utilization = 100%
- 1000M and 100M case
Best Regards,