Part Number: DS90UB928Q-Q1
Other Parts Discussed in Thread: DS90UR241
Their size and pinout are identical, so what's their differences in application? UB924 is said to be compatible with UB921, UB947 and UB949. UB928 is not compatible with them? If in our application the serializer is UR905, UB927 or UB925, which one is better of the two? Or, are they direct replacement to each other in our application?